QGH1336303-05

Application

Your device can be used for dual source accounting applications that involve two energy registers, for example Utility vs Genset, Utility vs Solar, Utility vs Wind, or a combination of any two-power source.

Your device can also be used in installations that require split energy monitoring for two conditions, for example, running and idle. You can form a relay to control the load in event of abnormalities such as excessive power consumption or electric faults.

The meters can be used for secondary billing application in large commercial complexes or buildings as tenant meters in custom panels, switch boards, switch-gear, Gen-set panels, non-renewable energy panels, and OEM panel boards.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?