QGH1336303-05

DM page (PM1130H only)

To view DM parameters:

  1. From the Home page, use Up or Down button to navigate to DM.
  2. Press OK.
  3. Press the Up or Down button to navigate to the next DM parameter.
  4. Press Left button to exit.
Name on display Description
d.W Displays the last demand value for active power.
d.VA Displays the last demand value for apparent power.
d.VAR Displays the last demand value for reactive power.
Rd Displays the raising demand value.
tR Displays the time remaining, for example: mm:ss
NOTE: Time remaining is displayed with 2 digit Minutes and 2 digit Second.
md.u Displays the max demand value for utility.
md.oc Displays the max demand occurrence time for utility.
md.G Displays the max demand for alternate source.
md.oc Displays the max demand occurrence time for alternate source, for example hhhhhh:mm
NOTE: Max demand occurrence time is displayed with 6 digit Hours and 2 digit Minutes.
NOTE: Based on the selected power type under Demand setup, the DM page displays either DM W, DM VA, or DM VAR.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?