QGH1336303-05

Demand (PM1130H)

The meter provides last, present, and maximum (peak) demand values, and a timestamp through counters when maximum (peak) demand occurred.

The meter supports standard demand calculation methods, including sliding block, fixed block, and rolling block.

Peak demand registers can be reset manually (password protected) or through communication.

Demand measurements include:

  • Demand (Total): W, VAR, VA

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?