QGH1336303-05

THD page (PM1130H only)

To view THD parameters:

  1. From the Home page, use Up or Down button to navigate to THD.
  2. Press OK.
  3. Press the Up or Down button to navigate to the next THD parameter.
  4. Press Left button to exit.
Name on display Description
V% 12, 23, 31 Displays the voltage THD% for Voltage lines 12, 23, and 31 respectively
V% 1, 2, 3 Displays the voltage THD% for Voltage lines 1, 2, and 3 respectively
A% 1, 2, 3 Displays the current THD% for current lines 1, 2, and 3 respectively
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?