DOCA0176EN-09

Overview

The Service Interface with part number LV485500 is a portable instrument for field testing.

The Service Interface is used:

  • For configuration of Enerlin'X devices.

  • For testing and configuration of MicroLogic trip units mounted in the following low voltage circuit breakers:

    • MasterPacT NT/NW circuit breakers

    • EasyPacT MVS circuit breakers

    • ComPacT NS circuit breakers

    • PowerPacT P- and R-frame circuit breakers

    • ComPacT NSX circuit breakers

    • PowerPacT H-, J-, or L-frame circuit breakers

NOTE:
  • The information related to the new generation of ComPacT NSX and PowerPacT H-, J-, and L-frame circuit breakers in this guide applies to the existing range ComPact NSX and PowerPact H-, J-, and L-frame circuit breakers also. The exceptions are mentioned wherever applicable.

  • The information related to the new generation of ComPacT NS and PowerPacT P- and R-frame circuit breakers in this guide applies to the existing range ComPact NS and PowerPact P- and R-frame circuit breakers also. The exceptions are mentioned wherever applicable.

  • These new ranges are based on the same technical and dimensional architecture as that of the existing range of circuit breakers.

EcoStruxure Power Commission is a global software with test functions features for testing the circuit breakers and communication accessories through the Service Interface.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.