DOCA0176EN-09

Firmware Version 001.000.000

New Features

The Service Interface can be used for testing the following MicroLogic trip units:

  • non-communicating MicroLogic trip units

  • communicating MicroLogic A, E, P, and H trip units

when they are mounted in the following low voltage circuit breakers:

  • MasterPacT NT/NW circuit breakers

  • EasyPacT MVS circuit breakers

  • ComPacT NS circuit breakers

  • PowerPacT P- and R- frame circuit breakers

The following tests can be performed using the Service Interface:

  • Automatic trip curve tests

    • with preconfigured test points

    • with custom test points

  • Zone-Selective Interlocking (ZSI) test

  • Device check up (Force trip test)

  • Preparation for primary injection tests:

    • Reset thermal memory

    • Inhibit ground-fault protection

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.