DOCA0176EN-09

Firmware Version 001.001.015

New Features

The Service Interface can be used for testing and configuring the MicroLogic 5.2 B and 5.3 B trip units mounted in the following low voltage circuit breakers:

  • ComPacT NSX circuit breakers

  • PowerPacT H-, J-, and L-frame circuit breakers

The following tests can be performed through the Service Interface:

  • Automatic trip curve test with pre-configured test points

  • Automatic trip curve test with custom test points

The Service Interface can be used for configuring the MicroLogic 5 A/E, 6 A/E, and 7 E trip units mounted in the following low voltage circuit breakers:

  • ComPacT NSX circuit breakers

  • PowerPacT H-, J-, and L-frame circuit breakers

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.