DOCA0176EN-09

Firmware Version 001.001.025

New Features

The Service Interface can be used for updating firmware and testing the MicroLogic 5 A/E, MicroLogic 6 A/E, and MicroLogic 7 E trip units mounted in the following low voltage circuit breakers:

  • ComPacT NSX circuit breakers

  • PowerPacT H-, J-, and L- frame circuit breakers

The Service Interface can be used for testing the MicroLogic trip units mounted in the following low voltage circuit breakers:

  • ComPacT NSX circuit breakers

  • PowerPacT H-, J-, and L-frame circuit breakers

The following tests can be performed through the Service Interface:

  • Zone-Selective Interlocking (ZSI) test

  • Preparation for primary injection tests

The Service Interface can be used for updating firmware and configuring Enerlin'X devices.

Bugs Fixed

The following bugs are fixed:

  • Refinement in communication during injection tests being performed.

  • Rectification in trip time calculation.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.