DOCA0176EN-09

Firmware Version 001.001.052

New Features

The following status are added to test port LED in the Service Interface to identify the unsuccessful connection between Service Interface and circuit breakers:

LED indication

LED color

Status description

FLASH (every 2 s) Green

Unsuccessful connection between Service Interface and MicroLogic trip unit mounted in the following circuit breakers with a LV485512SP cable:

  • MasterPacT NT/NW circuit breakers

  • EasyPacT MVS circuit breakers

  • ComPacT NS circuit breakers

  • PowerPacT P- and R-frame circuit breakers

Blue

Unsuccessful connection between Service Interface and MicroLogic trip unit mounted in the following circuit breakers with a LV485513SP cable:

  • ComPacT NSX circuit breakers

  • PowerPacT H-, J-, or L-frame circuit breakers

Unsuccessful connection between Service Interface and an Enerlin'X device with a LV485514SPcable.

The possible reasons for unsuccessful connection are:

  • The cable is inoperative.

  • The cable is not properly connected to the trip unit.

  • The communication between the Service Interface and a trip unit or an Enerlin'X device is unstable.

For more information on the other test port LED status, refer to the Service Interface for MasterPacT NT/NW, ComPacT, PowerPacT, and EasyPacT Circuit Breakers - User Guide.

Bug Fixed

The following circuit breakers were not discovered in EcoStruxure Power Commission software, when the Service Interface was connected to the MicroLogic trip units 1.2, 1.3, 2.2, 2.3, 3.2, 3.3, 4.2, 4.3, or 4.3 AL, which are mounted in the:

  • ComPacT NSX circuit breakers

  • PowerPacT H-, J-, and L-frame circuit breakers

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.