DOCA0176EN-09

Firmware Version 001.000.003

Bugs Fixed

The following bugs are fixed:

  • Algorithm was not able to support different Mitop coils.

  • EcoStruxure Power Commission register mapping was incorrect for the circuit breakers manufactured prior to 2007.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.