Firmware Version 001.000.000
New Features
The Service Interface can be used for testing the following MicroLogic trip units:
-
non-communicating MicroLogic trip units
-
communicating MicroLogic A, E, P, and H trip units
when they are mounted in the following low voltage circuit breakers:
-
MasterPact NT/NW circuit breakers
-
EasyPact MVS circuit breakers
-
ComPacT NS circuit breakers
-
PowerPacT P- and R- frame circuit breakers
The following tests can be performed using the Service Interface:
-
Automatic trip curve tests
-
with preconfigured test points
-
with custom test points
-
-
Zone-Selective Interlocking (ZSI) test
-
Device check up (Force trip test)
-
Preparation for primary injection tests:
-
Reset thermal memory
-
Inhibit ground-fault protection
-