DOCA0176EN-07

Firmware Version 001.001.019

New Features

The Service Interface can be used for testing and configuring the MicroLogic 5 A/E, MicroLogic 6 A/E, and MicroLogic 7 E trip units mounted in the following low voltage circuit breakers:

  • ComPacT NSX circuit breakers

  • PowerPacT H-, J-, and L-frame circuit breakers

Automatic trip curve test with pre-configured test points can be performed through the Service Interface.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?