9080CT9601R08/21

Single-Pole Thermal-Magnetic Control Circuit Protectors

Single-Pole Type GCB Circuit Protector Blocks

A. Thermal-magnetic circuit protector

B. 14 different current ratings: 0.1–15 A

C. On-Off switch

D. Visible trip indication

E. Mounts on Class 9080 GH track and on DIN mounting track

NOTE: 9080GCB circuit protector blocks have solderless box lugs. They accept one CU 6.0 (10)–1.5 (16) wire (for example, the wire gauge conversion of 6.0 mm2 is (10) AWG).

Technical Data

Dielectric strength

1500 Vac

Insulation resistance

100 MΩ

Weight

Approximately 2.2 oz.

Terminals

Box lug type

Recommended tightening torque

8–10 lbf-in (0.9–1.1 N•m)

Approvals

UL File: E233026

CNN: QVN02

CE

CSA File: 025490 Class: 3211–07

FingersafeTM per DIN 57470

Yes

Maxiumum voltage rating

  • GCB01 through GCB70

  • GCB100 and GCB150

  • 250 Vac / 65 Vdc

  • 125 Vac / 65 Vdc

Maximum interrupting rating 200 A, but not exceeding 10,000% (100 times) rated current

Selection:

  1. Determine the inrush correction factor from the table Inrush Ratio Correction.

  2. Determine the temperature correction factor from the table Ambient Temperature Correction.

  3. Determine the sealed current of the load that is being protected.

  4. Multiply the sealed current by the two correction factors and choose the closest circuit protector.

NOTE: Choosing a circuit protector with a value lower than the calculated value might cause nuisance tripping, while choosing the larger might provide a protector that will not properly protect the load.

Example:

A solenoid with sealed current of 0.75 A, an inrush ratio of 1:6, and in an ambient temperature of 85 °F (29.4 °C):

  • 0.75 x 1.5 x 1.05 = 1.18

  • Choose the 1.2 A protector

The 9080GCB circuit protectors come standard with the track adapter for mounting on 9080GH track (replacement adapter is 9080GH64). Removal of this adapter permits mounting on 9080MH2●●, MH3●●, and AM1 track. See Mounting Tracks for a complete listing of available tracks.

Maximum Current Values

Maximum Current 

Internal Resistance ¾

Maximum Voltage

Single Pole Type

0.1

0.5

0.8

1.0

1.2

1.5

133

6.6

2.55

1.97

1.22

0.86

0 .49

0 .31

0 .20

0.10

0.80

0.30

250 Vac / 65 Vdc

GCB01

GCB05

GCB08

GCB10

GCB12

GCB15

2.0

2.5

3.0

4.0

5.0

7.0

GCB20

GCB25

GCB30

GCB40

GCB50

GCB70

10.0

15.0

<0.02

<0.02

125 Vac

65 Vdc

GCB100

GCB150

These maximum current values assume the use of insulated copper conductors with 167° F (75° C) temperature rating, and are calculated based on NEC Article 310, Table 310-16. In most cases this value is the maximum ampacity of that wire or combination of wires (as listed in the above table Maximum Current Values) which has the greatest current carrying capacity. The actual allowable current for a particular application is dependent on the number, size, insulation class and other characteristics of the wires used.

Inrush Ratio Correction

Inrush Ratio

1:1 to 1:4

1:5

1:6

1:7

1:8

Factor

1.3

1.4

1.5

1.6

1.7

Ambient Temperature Correction

Ambient Temperature

70 °F
(21.1 °C)

100 °F
(37.8 °C)

120 °F
(48.9 °C)

140 °F
(60 °C)

160 °F
(71.1 °C)

180 °F
(82.2 °C)

200 °F
(93.3 °C)

Factor

1.0

1.1

1.2

1.3

1.4

1.5

1.6

Tripping Time

Tripping time of the circuit protector is determined from the values in the table Tripping Time in Seconds at 70 °F (21.1 °C). Divide the circuit protector value by the temperature correction factor from the table Ambient Temperature Correction above to determine the actual rated current referenced in the table Tripping Time in Seconds at 70 °F (21.1 °C).

Tripping Time in Seconds at 70 °F (21.1 °C)

Percent rated current

100%

200%

300%

400%

500%

600%

1000%

2000% and greater

Tripping Time (seconds)

no trip

10–40

38

1.5–9

0.8–6

0.003–4

0.003–2

Max. 0.02

NOTE: When several protectors are channel mounted adjacent to each other, the “no trip” current will be 80% of rated current at 70 °F (21.1 °C).
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.