DOCA0236EN-00

System Requirements

The following components are required for communication via EtherNet/IP or Modbus TCP.

Component

Type and Version

EcoStruxure Control Expert Classic software

Classic V15.0 SP1

PSx DTM Library version

3.14.54

Schneider_Electric_TeSys_island_DTM_Library version

2.2.2 or later

Controller

BMEP58•••• logic controller

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?