DOCA0236EN-00

Adding TeSys island to the Project

Perform the below steps to add TeSys island to the project:

Step

Action

1

Click Tools > DTM Browser.

2

Right-click on the CPU name in the DTM Browser window and select ADD.

Result: The ADD window is displayed on the screen.

3

In the Protocol drop-down menu, select Modbus over TCP.

4

Select TeSys island device and click Add DTM.

Result: The device properties window is displayed on the screen.

5

In the Properties of device window, change the name of the device if required and click OK.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?