DOCA0236EN-00

Installing Function Blocks of TeSys island Library

Perform the below steps to install the function blocks of TeSys island library:

Step

Action

1

Download the latest EcoStruxure Control Expert 2021 – TeSys island Library.zip file from Schneider Electric Industry End Users and SI Campus.

2

Extract the zip file in the local hard disk.

3

Click Start > EcoStruxure Control Expert Classic > Types library update.

Result: Types library update window is displayed on the screen.

4

Click Browse button.

5

Browse the location of the extracted zip folder, select FAMILY.DSC file, and click Open.

6

Click Install family.

Result: The installation of the library file starts.

7

On successful installation of a family file, a message appears on the screen. Click OK.

8

Open EcoStruxure Control Expert Classic software. Click Tools > Types Library Manager.

Result: TeSys island Library 2021 is displayed under Libset V15.0 or later.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?