DOCA0236EN-00

Configuring the IP Address of the CPU

Perform the below steps to configure the IP address of the CPU:

Step

Action

1

Double-click the Configuration folder in the Project Browser window.

Result: The physical view of the device configuration is displayed on the screen.

2

Double-click the communication connectors of the PLC on the PLC bus window.

Result: The communication settings window of the PLC is displayed on the screen.

3

Click Security menu and perform one of the following steps as required:

  • Click Enforce Security to enable or disable the services.

  • Click Unlock Security to enable all services.

4

Click IP Configuration menu and set the IP address of the CPU according to the network.

Note: The IP address A has to be different than the Main IP address.

5

Click the Validate icon () on the toolbar.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?