DOCA0236EN-00

Uploading TeSys island Project to PLC via Ethernet Cable

Perform the below steps to upload the TeSys island project to PLC via Ethernet cable:

Step

Action

1

Click PLC > Set Address.

Result: The Set Address window is displayed on the screen.

2

Select the IP address of the PLC. Select the Media as TCPIP and click OK.

3

Click the Connect icon () on the toolbar.

Result: TeSys island is integrated into the project and connected to the PLC Modicon M580 with EcoStruxure Control Expert Classic software.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?