DUG_Sedna_SSO_01

About the device

The Connected Single Socket Outlet 16 A (hereinafter referred to as Socket Outlet) is a connected electrical outlet designed to manage and control electrical devices in a convenient and efficient manner. You can remotely control and monitor the energy consumption of the plugged-in load.

The Socket outlet is equipped with a temperature protection mechanism. When the Socket outlet is used with a high load over a long time, the mechanism can switch off the Socket outlet, help to ensure overheat protection.

The Socket outlet is equipped with an overload protection mechanism. When the Socket outlet is used with a high load (18 A and high), the mechanism can switch off the Socket outlet, help to ensure overload protection.

NOTE:
  • Do not connect any devices that depend on a permanent power supply

  • Do not mix different load types in the controlled socket

  • Do not use multi-sockets in the controlled socket

  • Do not use for EV charging

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?