DUG_Sedna_SSO_01

Selecting LED indicator mode

Using the Wiser app, you can select the LED indicator mode for easy identification of the device status.
To set the LED indicator modes:
  1. On the Home page, tap All devices > Connected Single Socket Outlet.
  2. On the device control panel page, tap Settings.
  3. Tap LED Indicator Mode (A) and select any one of the following:
    • Reverse With Load - The LED on the Socket Outlet is On when the device is Off
    • Consistent With Load - The LED on the Socket Outlet is On when the device is On
    • Always Off - The LED on the Socket Outlet is always Off
    • Always On - The LED on the Socket Outlet is always On

    For information on LED color during each modes, refer to LED Indication.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?