DUG_Sedna_SSO_01

Using the device

The Control Panel allows you to switch the Socket Outlet On and Off and monitor the energy consumption.

On the Home page, tap All devices > Connected Single Socket Outlet to access the control panel.

On the Socket Outlet control panel page, you can see the following:

  • Power (W) - The load value of the device connected to the Socket Outlet (A)

  • Day (kWh) - The total energy consumption of the device connected to the Socket Outlet per day (B)

    NOTE: The total energy consumption per day value will automatically reset to zero at 00:00 hrs everyday.
  • The current state of the Socket Outlet (C)

  • Schedule (D)

  • Consumption (E)

  • Settings (F)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?