DUG_Sedna_SSO_01

Switching On/Off the device using app

By using the Wiser app, you can switch On/Off the device.
To switch the device On/Off:
  1. On the Home page, tap the power button (A) to switch On/Off the Socket Outlet.

  2. Alternatively, you can navigate to the control panel of the device and tap to switch On/Off the Socket Outlet.
    NOTE: The control panel shows the current state of the Socket Outlet.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?