Troubleshooting
|
Symptom |
Possible cause |
Solution |
|---|---|---|
|
The Socket Outlet is not turning ON. |
The Socket Outlet is broken or it could be an alarm if the LED blinks red. |
First, power cycle the Socket Outlet and check if it works afterwards. If it is still not working, you can replace the Socket Outlet. |
|
When there is an alarm, the user cannot switch ON the output locally or remotely. LED blinks fast RED. |
Clear the Socket Outlet alarms. |
To clear the alarm, press and hold the push button for 4 seconds. After 4 seconds, the blinking will stop and the alarm will be cleared. You can use the Socket Outlet again. NOTE: Before clearing
the alarm, you must verify the reason for overcurrent fault and thermal
fault.
|