DUG_Sedna_SSO_01

Resetting the device

You can reset the device to factory default manually.
To reset the device:
  1. Short press the push button 3 times (< 0.5 s) and then long press the push button once (>10 s).
  2. After 10 s, LED starts blinking red then release the push button.
    The LED stops blinking upon successful reset of the device.
  3. The Socket Outlet restarts and blinks green for a few seconds.
    NOTE: After reset, the LED turns amber, indicating that the socket is ready for pairing.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?