DUG_SysM/SysD_FLS_WSE–02

Pairing device with auto scan

Pairing the device with auto scan automatically discovers the device when the corresponding device is powered On.
Follow the steps to pair the device:
  1. On the Home page, tap +.
  2. Tap Auto scan tab and tap Confirm.
  3. If you have multiple hubs, do Step 4 or proceed to Step 5.
  4. Tap Select hub and select the Wiser hub from the slide-up menu.
  5. Short press the top right key 3 times to start pairing.
    NOTE: Wait for a few seconds until the device search is completed.
  6. Tap Next (A) and select Freelocate Switch.

  7. Once the device is added successfully, tap Done.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?