DUG_SysM/SysD_FLS_WSE–02

Using the device

The control panel of the Wireless Switch allows you to add lighting group, shutter group and moment to each push button.
On the Wireless Switch control panel, you can see the following:
  • Battery level (A)

  • Top left key (B)

  • Top right key (C)

  • Bottom left key (D)

  • Bottom right key (E)

NOTE: The app assigns both top and bottom keys to a lighting and shutter group, while any one key is assigned to a moment.
Functions of the Wireless Switch push button:

Group

Devices

Push button function

Lighting group

Switch

  • Turn On: Single press top key

  • Turn Off: Single press bottom key

Dimmer

  • Turn On: Single press top key

  • Turn Off: Single press bottom key

  • Increase brightness: Long press top key

  • Decrease brightness: Long press bottom key

Shutter group

Shutter

  • Open: Long press top key

  • Stop opening: Single press top/bottom key

  • Close: Long press bottom key

  • Stop closing: Single press top/bottom key

Moment

Triggers the devices that are added in a moment

  • Turn On: Single press the key

NOTE: You cannot turn off a moment. To go back to it’s previous state, you need to create another moment for that.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?