DUG_SysM/SysD_FLS_WSE–02

Removing the device

Using the Wiser app, you can remove a device from the device list.
To remove the device:
  1. On the Home page, tap All devices > Connected Wireless Switch 2-gang.
  2. Tap to display more details.
  3. Tap Remove and Factory Reset Device (A) and short press the top-right push button 3 times to activate the device.

    TIP: Alternatively, on the home page you can tap and hold the Connected Wireless Switch to remove the device.
    NOTE: By removing the device, you will reset the device. If you still have a problem with the reset, refer to resetting the device.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?