DUG_SysM/SysD_FLS_WSE–02

Pairing the device

Using the Wiser app, first pair your device with the Gateway to access and control the device. You can either add the device manually or do an auto-scan to pair it.
NOTE: If you want to change the Wireless Switch from 1-gang to 2-gang mode, then refer to Changing Wireless Switch from 1-gang to 2-gang before you start pairing.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?