DUG_SysM/SysD_FLS_WSE–02

Unbinding a lighting group

Unbinding the lighting group allows you to remove the lighting group from the assigned keys without deleting the lighting group.
Follow the steps to unbind a lighting group:
  1. Go to the control panel and tap Top left key.
  2. Tap Unbind.
  3. Short press the top right push button 3 times on the Wireless Switch to activate the device and tap Confirm on the app.

    The lighting group is now removed from the top and bottom left key.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?