DUG_SysM/SysD_FLS_WSE–02

Creating a moment

Follow the steps to create a moment:
  1. On the Home page, tap .
  2. Go to Moment > + icon to create a moment.
  3. Tap Edit name, enter the group name (A) and tap Save.
    TIP: You can choose the cover image that represents your moment by tapping .

  4. In the Action section, tap Add task (B) to open the slide-up menu.
  5. In the Add task menu, you can do either or all of the following actions (C):
    • Run the device - Select the devices that you want in a moment.
    • Delay - Set the delay time.
    NOTE: You can add one or more actions using .

  6. Tap Run the device and select the devices and its function you want to add and tap Next.
    EXAMPLE: If you want to open a curtain, then tap Curtain Switch > Control > Open and tap Save.
  7. Once all the actions are set, tap Save.
    TIP: Alternatively, you can navigate to Connected Wireless Switch 2-gang > Top right key > Moment and tap + icon to create a moment.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?