DUG_ITRV_WSE-01

Creating a schedule

The heating system is fully controlled and triggered by your schedule. Once the schedule is set, your system will follow the active schedule. You can create or modify the schedules at any time.
To create a schedule:
  1. On the Home page, tap All devices > Radiator Thermostats.
  2. Tap Schedule > Add Schedule to add a schedule.
  3. Set the time (A).
  4. Tap Repeat (B), select the days you want to set the schedule.
  5. Tap Note (C), enter the note and tap Confirm.
  6. Tap the toggle switch (D) to turn on the Notification for the schedule. The app will send a notification that the scheduled task is executed at the time of schedule.
  7. In the Radiator Thermostats section, you can adjust the temperature (E) for the scheduled time.
  8. Tap Save.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?