DUG_ITRV_WSE-01

Setting the room temperature manually

The room temperature can be increased/decreased manually by turning the cap of the thermostat.

Turn the thermostat cap:

  • In the “+” direction to increase the temperature setpoint. The red LED will light up for 5 seconds.

  • In the “-” direction to lower the temperature setpoint. The blue LED will light up for 5 seconds.

When the thermostat cap is turned, the setpoint temperature is increased/decreased by 2 °C from the current room temperature setpoint. The boost is active for 1 hour.

NOTE: If the setpoint temperature is already more than 2 °C above or below the room temperature, a boost will not change the setpoint temperature.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?