DUG_ITRV_WSE-01

About the device

The Wiser Radiator Thermostat (hereinafter referred to as Thermostat) uses integrated temperature sensors to control the flow of water through a radiator, thereby regulating the temperature in a room. The target temperature and the switching times are set in the Wiser app.

Personalize your home heating by adding a Thermostat to your Wiser system. This provides aneffortlesscontrol to set different schedules and temperatures in different rooms, and upgrading to room-to-room heating control couldsave 18% on energy usage. Thermostats provide ultimate comfort, convenience and practicality.

Intended use:

  • Individual room control

  • Mobile control anytime, anywhere with the Wiser app

  • Boost mode for ease and comfort

Diagram of operating elements

  1. 3 status LEDs

  2. Twistable cap

  3. Chrome ring nut

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?