DUG_ITRV_WSE-01

When the setpoint is higher than current temperature

When the setpoint (max 30 °C) is higher than the current temperature value, the flame icon on the control panel page will be displayed in highlighted state (A).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?