DUG_ITRV_WSE-01

Using the boost mode

Using the boost mode, the setpoint is increased by 2 ºC from the current room temperature.
Tto use the boost mode:
  1. On the Home page, tap All devices > Radiator Thermostat.
  2. On the device control panel page, select the .
  3. In the slide-up menu, select the Boost Duration (A) and tap Confirm.
    NOTE:
    • The boost duration is set to 1 hour by default.

    • The sliding bar can be used during the boost mode.

    • The boost mode will stop automatically when the boost duration is completed.

    • If the current temperature is 28.5 ºC - 29.5 ºC, then the boost mode will set the temperature to the maximum (30 ºC) temperature.

  4. To turn off the boost mode manually, go back to the control panel page and tap .
  5. In the slide-up menu, tap Off (B) and tap Confirm.
    NOTE: The Boost mode will be turned off if you manually adjust the device's setpoint or change the temperature through the app's sliding bar below the current temperature.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?