DUG_ITRV_WSE-01

For your safety

NOTICE
RISK OF DAMAGE TO DEVICE
• Make sure that the O-ring is seated firmly on the thread.
• The ring nut should be tightened by hand, do not use any tools. Do not tighten too hard.
Failure to follow these instructions can result in equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?