DUG_ITRV_WSE-01

Setting the room temperature using app

By using the Wiser app, the room temperature can be increased/decreased.
NOTE: You can only adjust the room temperature through the control panel of the group Thermostat.
  1. On the Home page, tap All devices > Radiator Thermostats.
  2. On the control panel page, you can do either of the following to adjust the temperature (A):
    • Tap “+” or “” sign to increase/decrease the temperature setpoint.
    • Drag the sliding bar up/down to increase/decrease the temperature setpoint.

  3. If you drag the sliding bar to bottom position, the control panel page will display the device as OFF (B), but the device will operate with a setpoint of 4 °C.
    NOTE:
    • The iTRV setpoint temperature ranges from 4 °C to 30 °C.

    • Each “+/–” tapping will increase or decrease the setpoint temperature by 0.5 °C.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?