Overview of the Wiser™ system
The Hub Wiser Hub Wiser gateway is the center of the system, processing control requests and status reports for connected Wiser devices.
Use the Wiser by SE app to set up the Wiser system, control Wiser devices and receive notifications.
With a personal account and the Wiser by SE app on a mobile phone/tablet, users can control Wiser devices in their home from any location where internet is available for both mobile phone/tablet and the Hub Wiser Hub Wiser gateway.
Within the home, Wiser devices can also be controlled using a Wiser AvatarOn freelocate.
Within the home, the devices, such as, LK FUGA® Wiser wireless battery 4 button switch, LK FUGA® Wiser wireless double relay, LK FUGA® Wiser wireless dimmer can be used to control the Wiser system.
The Iconic connected switches, dimmers and sockets leverage both BLE (Bluetooth Low Energy) and Zigbee technology, making them flexible and scalable. Iconic connected devices in BLE default mode can be swapped to Zigbee mode after installation to allow the smart home to evolve over time with the changing needs of the end user.
The intention of this document is to provide the information about the Zigbee System Commissioning. For more information on control with BLE, refer to clipsal.com/support pdl.co.nz/support .
For Sweden: For Spain: Visit: https://www.clipsal.com/wiser/welcome https://www.pdl.co.nz/wiser/welcome https://www.se.com/es/es/product-range/65750-wiser/?preferredCountry=yes
For Finland: Visit https://www.se.com/fi/fi/home/smart-home/local/wiser/homeowner.jsp?gclid=Cj0KCQjw1_SkBhDwARIsANbGpFsh9idRdWTx_RyGaiwYMTkXkzeYhbapV9ltJpk_wzgf8uJGqZ4GCgkaAtlrEALw_wcB.
For Portugal: Visit https://www.se.com/fi/fi/home/smart-home/local/wiser/homeowner.jsp?gclid=Cj0KCQjw1_SkBhDwARIsANbGpFsh9idRdWTx_RyGaiwYMTkXkzeYhbapV9ltJpk_wzgf8uJGqZ4GCgkaAtlrEALw_wcB
For Spain: Visit: https://www.clipsal.com/wiser/welcome https://www.pdl.co.nz/wiser/welcome https://www.se.com/es/es/product-range/65750-wiser/?preferredCountry=yes
For Portugal: Visit https://www.se.com/fi/fi/home/smart-home/local/wiser/homeowner.jsp?gclid=Cj0KCQjw1_SkBhDwARIsANbGpFsh9idRdWTx_RyGaiwYMTkXkzeYhbapV9ltJpk_wzgf8uJGqZ4GCgkaAtlrEALw_wcB