SUG_Wiser_Hungary_WSE-05

Ethernet mode connection- Gateway

  1. Locate the Ethernet port (A) on the gateway.
  2. Connect an Ethernet cable between the gateway and the router to suit the installation method used for the gateway:
    • Wall box installation (B)

    • Wall mount using two screws (C)

    • Table mount using optional Docking Kit (D)

You must add the gateway to the app before you can add devices to control them. To do this, first download and install the app on your mobile phone/tablet (see Downloading the app ) and register a user account. You can then add the gateway and optionally connect the gateway to the network router by Wi-Fi.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.