SUG_Wiser_Hungary_WSE-05

Differences between Moments and Automations

There are some features common to both Moments and Automations. Other features apply to only one or the other.

Moment settings and Automation settings pages in the app

Feature

Description

Moment

Automation

(See A) Name and background

Choose a unique name and set a custom background from a preset selection, your camera or photo albums.

Yes

Yes

(See B) Action* (* The Action consists of one or more tasks.)

Execute an automation.

No

Yes

Enable or disable a moment or automation (for example, if you are going away for an extended time).

Yes

Yes

Send a notification when the automation is triggered.

No

Yes

Set a delay time for the moment/automation to operate once triggered.

Yes

Yes

Select a device and configure settings to be applied when the moment/automation is triggered.

Yes

Yes

(See C) Show on home Page

Display a moment on the home page (tap the moment to operate).

Yes

No

(See D) Conditions

Trigger an automation based on one or more conditions, including temperature/humidity/weather, time (including sunset/sunrise at a nominated location), and device operation or output.

No

Yes

(See E) Effective Period

Configure when an automation can be triggered. Options include daytime and night based on a home location, a custom time period, and repeating on days of the week.

No

Yes

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.