SUG_Wiser_Hungary_WSE-05

Start a new Automation

To trigger one or more devices when selected conditions occur, create an Automation.
  1. In the Home page, tap the(A) icon.
  2. In the Moment page, tap the Automation tab (B) and then tap the + icon (C).
  3. Set a name for the Automation (for example, Welcome) (D) and optionally a background image (E).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.