SUG_Wiser_Hungary_WSE-05

Wiser Smoke Alarm 230 V / Wiser Smoke Alarm - Battery

Issue

Resolution/Action

Device does not sound when tested

  1. Confirm that the power switch is in ON position, or the device is installed correctly. If you are unsure then remove and reinstall the device.

  2. Press Test/Hush button until an alarm sound is produced. Do not press consecutively.

  3. If the problem persists or if you have questions about the warranty, contact customer care center.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.