SUG_Wiser_Hungary_WSE-05

Wireless Switch

Symptom

Possible cause

Solution

The Wireless Switch displays offline in the app.

The Wireless Switch battery may be low or drained.

Replace the battery in the device — refer to Free Located Wireless Switch 1-gang/ 2-gang user manual for replacing the battery (See the user manual link in ).

The Wireless Switch battery is disconnected from the network.

Press any push button on the Wireless Switch.

NOTE: The first press does not trigger Wireless Switch operation.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.