SUG_Wiser_Hungary_WSE-05

Resetting the gateway

Delete existing settings from a gateway for installation or to remove a gateway from the system. It may also be necessary to restore the gateway .

The reset/eject tool gateway is required to press the ‘R’ button.

There are two reset options:

  • Level 1 reset (Restores Ethernet/WLAN settings only).
  • Level 2 reset (Upon successful reset, all configuration data, user data, and network data is deleted).
  1. (See A) Locate the Reset button on the side of the gateway.
  2. Do one of the following:
    • Level 1 reset: Press and hold the Reset button for 5 s (max. 15 s).

      The Ethernet LED (B) and WLAN LED (C) both flashes once.

    • Level 2 reset: Press and hold the Reset button for more than 15 s.

      The Ethernet LED (B) and WLAN LED (C) both flashes 3 times.

  3. Release the Reset button.

The gateway restarts. This takes about 40 s.

After a Level 2 reset, all settings are returned to their original default values. The latest Zigbee firmware is also downloaded from the current active host and installed, erasing any existing network settings.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.