SUG_Wiser_Hungary_WSE-05

Sensors

Wiser Window/Door Sensor

Detects when windows and doors are opened or closed and sends the status to the gateway.

Instruction Sheet (PDF)

Device User Guide

Wiser Motion Sensor

Reports the detection of movement to the Wiser Hub (and device to perform configured functions), measures the luminance of the environment and passes this data to the Wiser Hub. The threshold of luminance settings and/ or detection of movement can be programmed to determine what action to be taken at that moment.

Instruction Sheet (PDF)

Device User Guide

Wiser Water Leakage Sensor

When the sensor is connected to the Wiser gateway and detects water on the floor, the sensor sends out a sound alarm and reports the event to the gateway.

NOTE: The device can operate as a standalone product when not connected to the gateway. This device also produces sound alarm when not connected to thegateway.

Instruction Sheet (PDF)

Device User Guide

Wiser Temperature/Humidity Sensor

Maintains a comfortable environment in the home by detecting changes in temperature and humidity and having the Wiser system respond by adjusting connected environmental control systems, such as, automatically turning on an air conditioner if the temperature is high or turning on an exhaust fan if the humidity is high.

Instruction Sheet (PDF)

Device User Guide

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.