SUG_Wiser_Spain_Portugal_WSE-08

Device LED behavior

Devices have LEDs to indicate their operating status and to confirm actions such as resetting or joining a network.

Gateway

Status

LED Indication

LED Indication Duration

Switching On/Restarting

All 3 LEDs display solid white

40 s

Connected to router (Wi-Fi)

WLAN LED displays solid white

While connected to router

Connected to router (Ethernet)

Ethernet LED displays solid white

While connected to router

Zigbee network initialized

Zigbee network LED displays solid white

While Zigbee network is available

Zigbee network open for pairing (Wi-Fi)

WLAN LED displays solid white, Zigbee network LED blinks white

While Zigbee network is open

Zigbee network open for pairing (Ethernet)

Ethernet LED displays solid white, Zigbee network LED blinks white

While Zigbee network is open

Resetting Gateway

Reset Level

User Action

LED Indication

LED Indication Duration

Level 1 reset in progress. (Restores Ethernet/WLAN settings only)

Press and hold the Reset button for 5 to 15 seconds

Ethernet/WLAN LEDs blink white.

LEDs blink once.

Level 2 reset in progress. (Upon successful reset, all configuration data, user data, and network data is deleted).

Press and hold the Reset button for more than 15 seconds

Ethernet/WLAN LEDs blink white.

LEDs blink 3 times.

Pairing

Device

User Action

LED Indication

Status

Sensors, Micro modules, Dimmers, Switches, Motion sensor switch, Motion sensor dimmer, SmartPlug, Blinds control, Wireless switch

Press the push button 3 times

LED blinks orange, once per second.

Pairing mode is active for 30 seconds. When pairing is completed, LED displays solid green for a time, before turning Off.

IP camera Indoor

Plug-in the power cable to power on the device

After a few seconds LED starts blinking red for pairing.

LED glows green, when the pairing mode is complete.

IP Camera Outdoor

Plug-in the power cable to power on the device

After a few seconds LED starts blinking red for pairing.

  • LED blinks blue, when searching for Wi-Fi mode

  • LED glows blue, when connected to Wi-Fi

Wiser IR Convertor

Device

Status

LED Indication

Duration

Wiser IR Convertor

Connection in progress

Flash orange

Until connection completed

Connection completed/connected to network

Solid green

5 s

Reset in progress

Flash red

Until Reset/Prog button released

Reset completed

Solid orange

5 s

Power indication

Device

User Action

LED Indication

Status

SmartPlug

No action

LED displays solid red.

SmartPlug power is On.

Resetting smart devices

Device

User Action

LED Indication

Status

Sensors, Micro modules, Dimmers, Switches, Motion sensor switch, Motion sensor dimmer, SmartPlug, Blinds control

Press the push button 3 times and hold it down once for > 10 s.

After 10 s, the LED starts blinking red.

The device is in reset mode. It is reset to the factory settings after 10 seconds. The device then restarts and the LED starts blinks green, before turning Off.

Connected sockets

Status

LED Indication

Description

Setting 1 (Default state)

The Red LED glows.

  • The Red LED glows when the output is switched ON

  • The LEDs are OFF, when the output is OFF.

All the LEDs are OFF.

Setting 2

The Red LED glows

  • Red LED is ON when output is ON.

  • Green LED is ON when output is OFF.

The Green LED glows

Setting 3

All LEDs are OFF

  • All LEDs are OFF, when the output is OFF.

  • Green LED is ON when output is OFF.

Green LED is glows

Setting 4

All LEDs are OFF

There will be no LED indication in any case of the output state.

NOTE: Above settings are done in the app.

Smoke Alarm Battery/Wiser Smoke Alarm 230 V

Pairing

User Action

LED Indication

Status

Press the Setup/Reset button 3 times

LED blinks yellow, once per second.

Pairing mode is active for 30 seconds. When pairing is completed, LED glows green for some time before turning Off.

Resetting

User Action

LED Indication

Status

Press the Setup/Reset button 3 times and hold it down once for > 10 s.

After 10 s, the LED starts blinking red.

The device is in reset mode. It is reset to the factory settings after 10 seconds. The device then restarts and the LED starts blinks green before turning Off.

Operating

Operating Mode Standby LED Alarming Sound Duration

Normal mode / Standby mode

Blinks every 48 s

OFF

Alarm Mode

Local Alarm *

Blinks every 1 s

3 beeps every 4 s

Interconnected alarm

OFF

3 beeps every 4 s

Test mode

1 blink every 1 s

3 beeps every 4 s

Until Test/Hush button is released

RF interconnection test

OFF

Continuous 3 beeps every 4 s

25 s

Hush mode

Blinks every 8 s

OFF

10 min

Low battery mode

Blinks every 48 s

1 beep every 48 s

End of life: replace smoke alarm

Fault mode

2 blinks every 48 s

2 beeps every 48 s

Until fault has been cleared

Snooze Mode

Low battery

Blinks every 24 s

OFF

10 hrs

Fault

2 blinks every 24 s

OFF

10 hrs

Alarm memory

Blinks every 48 s

OFF

10 hrs

NOTE: For all the operating modes, LED blinks Red.

* Local smoke alarm all Red LEDs blink and for Local temperature alarm only Standby Red LED blinks.

Wiser Flush-mounted Thermostat 2 A

Pairing the device

Status

User Interaction

Description

Pairing in progress

The thermostat matrix display flashes "Jn" to indicate joining is initiated when the thermostat rotary push-button is pressed and held for > 3 s.

Successful joining network

The thermostat matrix display flashes a green LED when the thermostat successfully joins a network.

Fails to join the network

The thermostat matrix display flashes a red LED when the thermostat fails to join the network.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.