SUG_Wiser_Spain_Portugal_WSE-08

Heat device

Wiser Flush-mounted Thermostat 2 A

The Wiser Flush-mounted Thermostat 2 A is mainly used for water-based heating and cooling applications, such as water-based underfloor heating and radiator heating.

NOTE:The thermostat is not suitable for directly connecting an electrical heating.

Instruction Sheet

Device User Guide

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.