SUG_Wiser_Spain_Portugal_WSE-08

User interfaces

Connected push-button module, 1-gang/2-gang

With the Connected push-button module you can carry out various functions, depending on the insert, such as:

  • Switching, dimming and controlling blinds

  • Retrieving, changing and saving light scenes and blind scenes

NOTE: The application modules must be used when System M and System Design wiring device is used.

Instruction Sheet (PDF)

Device User Guide

Connected wireless switch 1-gang/2-gang

The Connected wireless switch 1-gang/2-gang is used to control a group of Zigbee devices within the same Zigbee network.

The device can be configured through the Wiser app or can be paired with other Wiser Zigbee devices.

Instruction Sheet (PDF)

Device User Guide

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.