SUG_Wiser_Spain_Portugal_WSE-08

Switches

Symptom

Solution

Connected load does not switch on.

  • Check the power supply.

  • Turn the device off and back on again.

  • Check the load.

  • In the case of an external push button, check the wiring.

  • Re-couple devices.

Connected load is switched on permanently.

Reduce the Detection Delay time in the app.

NOTE: This setting is only available in SmartMove Relay.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.