SUG_Wiser_Spain_Portugal_WSE-08

System requirements

To use the app, your mobile phone must support particular operating systems and versions.

Supported operating systems:

  • Android™ OS version 7 and above
  • Apple® iOS 11 and above
NOTE:
  • When a new version of an operating system is released, it may take some time before the Wiser system is fully compatible with that version.

  • Using Schneider Electric applications with an Android phone that has bypassed restrictions, or a jailbroken iPhone, voids all warranties associated with the application.

  • The compatibility of the interfaces with mobile phones depends on the software version installed on your mobile phone, and may change with a software upgrade. Due to the large number of mobile phones available in the market, the compatibility and functionality of your mobile phone with the app cannot be guaranteed.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.